1.3.5.3.36 MAC_DATA_INDICATION_CB Function Pointer
C
typedef void (*MAC_DATA_INDICATION_CB)(uint16_t conHandle, uint8_t *data,
uint16_t dataLen, uint32_t timeRef);
Summary
Callback function pointer for the MAC data indication.
Description
This callback is used for the MAC data indication.
- conHandle - Unique identifier of the connection
- data - Pointer to data to be received through this connection
- dataLen - Length of the data in bytes
- timeRef - Time reference (in 10s of microseconds) (v1.4)
Remarks
None.