1.3.5.3.3 MAC_Tasks Function
C
void MAC_Tasks(void);
Summary
Maintains the MAC layer state machine.
Description
This function is used to maintain the MAC layer internal state machine and generate callbacks.
Precondition
The MAC_Initialize function should have been called before calling this function.
Parameters
None.
Returns
None.
Example
while (true)
{
MAC_Tasks();
}
Remarks
This function must be periodically called by the user application through the PRIME Stack.