10.3.4.77 ATPL360_REG_RX_CHN_EST_REAL (0x4045)
Real part of Channel Estimation of the last received PDU. For each
carrier in the PRIME channel, there is one 2-byte signed value. The PL360 PHY layer
computes the Channel Estimation from the header symbols, which is used for the
demodulation of payload symbols. The value has no unit and the scale does not reflect
the real received signal level, although the RSSI (uc_rssi_avg in PHY-DATA.indication) could be used to
scale the Channel Estimation and obtain the RSSI per carrier in the working band.
If Double Channel is used (ATPL360_REG_NUM_CHANNELS (0x403D)), another array is needed for the second channel (ATPL360_REG_RX_CHN_EST_REAL_2 (0x4047)).
Access: Read-only.
Value Range: 194 bytes.
Default Value: All 0s.