2.3.69 ADCx_ChannelResultIsReady Function
C
// x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
inline static bool ADCx_ChannelResultIsReady(ADCx_CHANNEL channel);
Summary
Returns the status of conversion and determine if conversion is completed.
Description
This inline function returns the status of conversion.This function is used to determine if conversion is completed. When conversion is complete the function returns true otherwise false.
Precondition
ADCx_SoftwareTriggerEnable() function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| channel | Selected channel |
Returns
true - Conversion is complete.
false - Conversion is not complete.
Example
bool status; status = ADC1_ChannelResultIsReady(ADC1_CHANNEL0);
Remarks
None.