2.3.15 ADCx_WindowModeSet Function
C
void ADCx_WindowModeSet(ADC_WINMODE mode); // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
This function configures the window comparison mode.
Description
This function sets the window comparison mode.
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
| Param | Description |
|---|---|
| mode | window comparison mode |
Returns
None
Example
ADC0_Initialize(); ADC0_WindowModeSet(ADC_WINMODE_GREATER_THAN_WINLT);
Remarks
None