2.3.72 ADCx_CompareStatusGet Function
C
// x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
inline static bool ADCx_CompareStatusGet(ADCx_CHANNEL channel);
Summary
Returns the status of the comparator.
Description
This function returns the status of the comparator.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| channel | Selected channel |
Returns
true - If Compare status is true
false - If Compare status is false
Example
bool cmpStatus; cmpStatus = ADC1_CompareStatusGet(ADC1_CHANNEL0);
Remarks
None