5.34.117.96 Example

The following code will determine if a design has been modified.

set bDesignModified [ is_design_modified ] if { $bDesignModified == 0 } {

puts “Design has not been modified.”

}

is_design_state_complete

is_design_state_complete value

Returns a Boolean value (0 for false, 1 for true) indicating if a specific design state is valid. True is returned if the specified design state is valid.