5.34.117.59 Arguments
-attribute{value}
This specifies the attribute for which the values will be applied. The following table shows the acceptable values for this argument:
Value | Description |
outdrive | Applies suggested outdrive values |
slew | Applies suggested slew values |
-io {value}
This selects the I/Os for which the suggestion will be applied. To select multiple I/Os, use -io {value} for each I/O.