5.34.117.29 Arguments
value
Must be one of the valid string values summarized in the table below:
Value | Description |
name | Design name. The result is set to the design name string. |
family | Silicon family. The result is set to the family name. |
design_path | Fully qualified path of the design file. The result is set to the location of the .adb file. If a design has not been saved to disk, the result will be an empty string. This command |
Value | Description |
replaces the command get_design_filename. | |
design_folder | Directory (folder) portion of the design_path. |
design_file | Filename portion of the design_path. |
cwdir | Current working directory. The result is set to the location of the current working directory |
die | Die name. The result is set to the name of the selected die for the design. If no die is selected, this is an empty string. |
Package | Package. The result is set to the name of the selected package for the design. If no package is selected, this is an empty string. |
Speed | Speed grade. The result is set to the speed grade for the design. If no speed grade is selected, this is an empty string. |