5.34.117.100 ExceptionsThe command will return an error if a design is not loaded.The command will return an error if more than one argument is passed.The command will return an error if the argument is not one of the valid values.