5.34.117.1 Arguments

-export_directory {value}

Specifies the directory name for the exported *.v, *.vhd, *.cxf and *.cdb files. Value is the path and name of the directory

-export_name "blockname"

Specifies the prefix of the exported *.v, *.vhd, *.cxf, and *.cdb files, where blockname is the name of the prefix.

-placement "value"

Exports placement information. Possible values:

Value

Description

yes

Exports the placement information. Specify "yes" only if the placer state is valid and -placement is specified as "yes."

no

Do not export the placement information.

-routing "value"

Exports placement information. Possible values:

Value

Description

yes

Exports routing information. Specify "yes" only if the routing state is valid and - placement is specified as "yes."

no

Do not export the routing information.

-comment "value"

Adds comments to document the block.

-export_language "value"

Specifies the export format of the CXF file for Libero IDE. Possible values:

Value

Description

VERILOG

CXF file is Verilog.

VHDL

CXF file is VHDL.

-region "value"

Option to publish all the user regions and make them available when you instantiate the block. Possible values:

Value

Description

YES

Publishes all the user regions, makes them available when you instantiate your block.

NO

Disables region publishing