5.10 Read
The READ instruction (03H) is supported in SPI mode only,
with a maximum clock frequency of 108 MHz. This command is not supported in QPI mode. Upon
execution, the device outputs data on SO/SIO[1], starting from the specified address, and
continuously streams data through successive addresses until the operation is terminated by
a low-to-high transition on CE#. The internal Address Pointer automatically increments
after each byte read. When the highest memory address is reached, the Address Pointer
returns to address location 000000H.
READ operation, the host issues the 8-bit
read command (03H), followed by three bytes. CE# must remain active-low for the duration of
the read cycle (see Figure 5-5 for the
read sequence).