6.11.139 nextafter Function
Determines the next value after x in the direction of y
that can be represented by a double precision floating-point value.
Include
<math.h>
Prototype
double nextafter(double x, double y);
Arguments
x- the original value
y- the target value
Return Value
Determines the next value after x in the direction of
y that can be represented by the type of the function. The value of
y is returned if x equals y.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x,y,z;
x = 150.0;
y = 300.0;
z = nextafter(x, y);
printf("The next representable value after %f in the direction of %f is %.10f\n", x, y, z);
x = 150.0;
y = -300.0;
z = nextafter(x, y);
printf("The next representable value after %f in the direction of %f is %.10f\n", x, y, z);
}
Example Output
The next representable value after 150.00000 in the direction of 300.00000 is 150.0000152588
The next representable value after 150.00000 in the direction of -300.00000 is 149.9999847412