6.11.126 lrintl Function
Returns the long double precision floating-point argument rounded to the nearest integer value.
Include
<math.h>
Prototype
long int lrintl(long double x);
Argument
x- the value to round
Return Value
Returns the value of x rounded to the nearest integer value using the
current rounding direction. The rounded integer is returned as a long
integer value.
Remarks
The value returned is unspecified if the rounded value is outside the range of the return type.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x;
long int y;
x = 10.103;
y = lrintl(x);
printf("The nearest integer value to %Lf is %ld\n", x, y);
x = 10.51;
y = lrintl(x);
printf("The nearest integer value to %Lf is %ld\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10
The nearest integer value to 10.510000 is 11