6.11.184 tgammal Function
Calculates the gamma function of a long double precision floating-point argument.
Include
<math.h>
Prototype
long double tgammal(long double x);
Argument
x- value for which to evaluate the gamma function
Return Value
Calculates the gamma function of the argument.
Remarks
If x is negative or if the result cannot be represented with
x is zero, a domain error will occur and errno
will be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
x = 0.5;
y = tgammal(x);
if(errno)
perror("Error");
printf("The gamma function of %Lf is %Lf\n", x, y);
x = -0.75;
y = tgammal(x);
if(errno)
perror("Error");
printf("The gamma function of %Lf is %Lf\n", x, y);
}
Example Output
The gamma function of 0.500000 is 1.772454
The gamma function of -0.750000 is -4.834147