6.11.5 acos Function
Calculates the trigonometric arc cosine function of a double precision floating-point value.
Include
<math.h>
Prototype
double acos(double x);
Argument
x- value between -1 and 1 for which to return the arc cosine
Return Value
Returns the arc cosine of x in the range radians (inclusive) or NaN if a domain error occurs.
Remarks
If x is less than -1 or greater than 1, a domain error will occur and
errno will be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x,y;
errno = 0;
x = -2.0;
y = acos (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
errno = 0;
x = 0.10;
y = acos (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
}
Example Output
Error: Domain error
The arccosine of -2.000000 is nan
The arccosine of 0.100000 is 1.470629