6.11.170 sinh Function
Calculates the hyperbolic sine function of a double precision floating-point value.
Include
<math.h>
Prototype
double sinh (double x);
Argument
x- value for which to return the hyperbolic sine
Return Value
Returns the hyperbolic sine of x.
Remarks
If x is too large, a range error will occur and errno will
be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = -1.5;
y = sinh (x);
if (errno)
perror("Error");
printf("The hyperbolic sine of %f is %f\n",
x, y);
errno = 0;
x = 0.0;
y = sinh (x);
if (errno)
perror("Error");
printf("The hyperbolic sine of %f is %f\n",
x, y);
errno = 0;
x = 720.0;
y = sinh (x);
if (errno)
perror("Error");
printf("The hyperbolic sine of %f is %f\n",
x, y);
}
Example Output
The hyperbolic sine of -1.500000 is -2.129279
The hyperbolic sine of 0.000000 is 0.000000
Error: range error
The hyperbolic sine of 720.000000 is inf