6.11.25 atanhl Function
Calculates the trigonometric arc hyperbolic tangent function of a double precision floating-point value.
Include
<math.h>
Prototype
long double atanh(long double x);
Argument
x- value for which to return the arc hyperbolic tangent
Return Value
Returns the arc hyperbolic tangent of x or NaN if a domain error
occurs.
Remarks
If x is not in the range , a domain error occurs and errno will
be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x, y;
x = 0.5;
y = atanhl(x);
printf("The arc hyperbolic tangent of %Lf is %Lf\n", x, y);
x = -1.0;
y = atanhl(x);
printf("The arc hyperbolic tangent of %Lf is %Lf\n", x, y);
}
Example Output
The arc hyperbolic tangent of 0.500000 is 0.549306
The arc hyperbolic tangent of -1.000000 is -inf