6.11.89 isgreaterequal Macro
Determines if its first argument is larger than or equal to its second.
Include
<math.h>
Prototype
int isgreaterequal(floating-point x, floating-point
y);
Argument
x- any floating-point number
y- any floating-point number
Return Value
Determines if x is larger than or equal to y, as if by
the expression (x) >= (y) only without any invalid floating-point
exception should the arguments be unordered (i.e. should one of them be NaN).
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y;
int b;
x = -5.7;
y = 2.0;
b = isgreaterequal(x, y);
printf("That %f is greater than or equal %f is %s\n", x, y, b ? "true" : "false");
}
Example Output
That -5.700000 is greater than or equal 2.000000 is false