6.11.22 atan2l Function
Calculates the trigonometric arc tangent function of
y/x.
Include
<math.h>
Prototype
long double atan2l(long double y, long double x);
Arguments
y- y value for which to return the arc tangent
x- x value for which to return the arc tangent
Return Value
Returns the arc tangent in radians in the range (inclusive) with the quadrant determined by the signs of both parameters.
Remarks
A domain error occurs if both x and y are zero.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y, z;
errno = 0;
x = 0.0;
y = 2.0;
z = atan2l(y, x);
if (errno)
perror("Error");
printf("The arctangent of %Lf/%Lf is %Lf\n", y, x, z);
errno = 0;
x = -1.0;
y = 0.0;
z = atan2l(y, x);
if (errno)
perror("Error");
printf("The arctangent of %Lf/%Lf is %Lf\n", y, x, z);
errno = 0;
x = 0.0;
y = 0.0;
z = atan2l(y, x);
if (errno)
perror("Error");
printf("The arctangent of %Lf/%Lf is %Lf\n", y, x, z);
}
Example Output
The arctangent of 2.000000/0.000000 is 1.570796
The arctangent of 0.000000/-1.000000 is 3.141593
Error: domain error
The arctangent of 0.000000/0.000000 is nan