6.11.36 cosf Function
Calculates the trigonometric cosine function of a single precision floating-point value.
Include
<math.h>
Prototype
float cosf (float x);
Argument
x- value for which to return the cosine
Return Value
Returns the cosine of x specified in radians in the range
. NaN is returned if x is
.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
errno = 0;
x = -1.0F;
y = cosf (x);
if (errno)
perror("Error");
printf("The cosine of %f is %f\n", x, y);
errno = 0;
x = 0.0F;
y = cosf (x);
if (errno)
perror("Error");
printf("The cosine of %f is %f\n", x, y);
}
Example Output
The cosine of -1.000000 is 0.540302
The cosine of 0.000000 is 1.000000