6.11.138 nearbyintl Function
Returns the double precision floating-point argument rounded to an integer value but returned in the argument's type.
Include
<math.h>
Prototype
long double nearbyintl(long double x);
Argument
x- the value to round
Return Value
Returns the value of x rounded to an integer value using
the current rounding direction and without generating an exception. The rounded integer
is returned as a floating-point value.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y;
x = 10.103;
y = nearbyintl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
x = 10.51;
y = nearbyintl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10.000000
The nearest integer value to 10.510000 is 11.000000