6.11.45 erfcf Function
Calculates the complementary error function of the argument.
Include
<math.h>
Prototype
float erfcf(float x);
Argument
x- upper limit of summation
Return Value
Returns the complementary error function of the argument, being 1 minus the error function of the same argument.
Remarks
A range error occurs if the x is too large and errno
will be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
float x, y;
x = 0.5;
y = erfcf(x);
printf("The complementary error function from 0 to %f is %f\n", x, y);
x = -0.75;
y = erfcf(x);
printf("The complementary error function from 0 to %f is %f\n", x, y);
}
Example Output
The complementary error function from 0 to 0.500000 is 0.479500
The complementary error function from 0 to -0.750000 is 1.711156