6.11.112 log10 Function
Calculates the base-10 logarithm of a double precision floating-point value.
Include
<math.h>
Prototype
double log10(double x);
Argument
x- any double precision floating-point positive number
Return Value
Returns the base-10 logarithm of x. If x is
0, infinity is returned. If x is a negative number, NaN is
returned .
Remarks
If x < 0, a domain error will occur and errno will
be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = 2.0;
y = log10 (x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
errno = 0;
x = 0.0;
y = log10 (x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
errno = 0;
x = -2.0;
y = log10 (x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
}
Example Output
The base-10 logarithm of 2.000000 is 0.301030
The base-10 logarithm of 0.000000 is -inf
Error: domain error
The base-10 logarithm of -2.000000 is nan