6.11.171 sinhf Function
Calculates the hyperbolic sine function of a single precision floating-point value.
Include
<math.h>
Prototype
float sinhf (float x);
Argument
x- value for which to return the hyperbolic sine
Return Value
Returns the hyperbolic sine of x.
Remarks
If x is too large, a range error will occur and
errno will be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
errno = 0;
x = -1.0F;
y = sinhf (x);
if (errno)
perror("Error");
printf("The hyperbolic sine of %f is %f\n", x, y);
errno = 0;
x = 0.0F;
y = sinhf (x);
if (errno)
perror("Error");
printf("The hyperbolic sine of %f is %f\n", x, y);
}
Example Output
The hyperbolic sine of -1.000000 is -1.175201
The hyperbolic sine of 0.000000 is 0.000000