6.11.115 log1p Function
Calculates the natural logarithm of a double precision floating-point value plus 1.
Include
<math.h>
Prototype
double log1p(double x);
Argument
x- any positive value for which to return the log
Return Value
Returns the natural (base-) logarithm of x+1 or NaN if a domain error occurs. The result
of log1p(x) is generally expected to be more accurate than that of
log(x+1) when the magnitude of x is small.
Remarks
If x is less than -1, a domain error will occur and
errno will be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = 2.0;
y = log1p(x);
if(errno)
perror("Error");
printf("The result of log1p(%f) is %f\n", x, y);
errno = 0;
x = 0.0;
y = log1p(x);
if(errno)
perror("Error");
printf("The result of log1p(%f) is %f\n", x, y);
errno = 0;
x = -2.0;
y = log1p(x);
if(errno)
perror("Error");
printf("The result of log1p(%f) is %f\n", x, y);
}
Example Output
The result of log1p(2.000000) is 1.098612
The result of log1p(0.000000) is 0.000000
Error: domain error
The result of log1p(-2.000000) is nan