6.11.134 nanf Function
Returns a quiet NaN single precision floating-point value.
Include
<math.h>
Prototype
float nanf(const char * tagp);
Arguments
tagp- an optional, implementation-defined string which might be used to represent extra information in the NaN’s significand
Return Value
The call nan("n-char-sequence") is equivalent to
strtof("NAN(n-char- sequence)", (char**) NULL); the call
nan("") is equivalent to strtof("NAN()", (char**)
NULL). When tagp does not point to an n-char sequence or
an empty string, the equivalent call to strtof would have a first
argument of "NAN".
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
float x;
z = nanf(NULL);
printf("Here is our not-a-number: %f\n", z);
}
Example Output
Here is our not-a-number: nan