6.11.38 cosh Function
Calculates the hyperbolic cosine function of a double precision floating-point value.
Include
<math.h>
Prototype
double cosh(double x);
Argument
x- value for which to return the hyperbolic cosine
Return Value
Returns the hyperbolic cosine of x. It returns infinity if
x is .
Remarks
If the magnitude of x is too large, a range error occurs, and
errno will be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = -1.5;
y = cosh (x);
if (errno)
perror("Error");
printf("The hyperbolic cosine of %f is %f\n", x, y);
errno = 0;
x = 0.0;
y = cosh (x);
if (errno)
perror("Error");
printf("The hyperbolic cosine of %f is %f\n", x, y);
errno = 0;
x = 720.0;
y = cosh (x);
if (errno)
perror("Error");
printf("The hyperbolic cosine of %f is %f\n", x, y);
}
Example Output
The hyperbolic cosine of -1.500000 is 2.352410
The hyperbolic cosine of 0.000000 is 1.000000
Error: range error
The hyperbolic cosine of 720.000000 is inf