6.11.79 frexpf Function
Gets the fraction and the exponent of a single precision floating-point number.
Include
<math.h>
Prototype
float frexpf(float x, int * exp);
Arguments
x- floating-point value for which to return the fraction and exponent
exp- pointer to a stored integer exponent
Return Value
Returns the fraction, exp points to the exponent. If
x is 0, the function returns 0 for both the fraction and
exponent.
Remarks
The absolute value of the fraction is in the range of 1/2 (inclusive) to 1 (exclusive). No domain or range error will occur.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
float x,y;
int n;
x = 0.15F;
y = frexpf (x, &n);
printf("For frexpf of %f\n the fraction is %f\n ", x, y);
printf(" and the exponent is %d\n\n", n);
x = -2.5F;
y = frexpf (x, &n);
printf("For frexpf of %f\n the fraction is %f\n ", x, y);
printf(" and the exponent is %d\n\n", n);
x = 0.0F;
y = frexpf (x, &n);
printf("For frexpf of %f\n the fraction is %f\n ", x, y);
printf(" and the exponent is %d\n\n", n);
}
Example Output
For frexpf of 0.150000
the fraction is 0.600000
and the exponent is -2
For frexpf of -2.500000
the fraction is -0.625000
and the exponent is 2
For frexpf of 0.000000
the fraction is 0.000000
and the exponent is 0