6.11.16 asinhl Function
Calculates the arc hyperbolic sine function of a double precision floating-point value.
Include
<math.h>
Prototype
long double asinhl(long double x);
Argument
x- value for which to return the arc hyperbolic sine
Return Value
Returns the arc hyperbolic sine of x.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = -1.0;
y = asinhl(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %Lf is %Lf\n", x, y);
errno = 0;
x = 1.0;
y = asinhl(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %Lf is %Lf\n", x, y);
errno = 0;
x = 720.0;
y = asinhl(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %Lf is %Lf\n", x, y);
}
Example Output
The arc hyperbolic sine of -1.000000 is -0.881374
The arc hyperbolic sine of 1.000000 is 0.881374
The arc hyperbolic sine of 720.000000 is 7.272399