6.11.142 nexttoward Function
Determines the next value after x in the direction of y
that can be represented by a double precision floating-point value.
Include
<math.h>
Prototype
double nexttoward(double x, long double y);
Arguments
x- the original value
y- the target value as a
long double
Return Value
Determines the next value after x in the direction of y
that can be represented by the double type. The value of
y converted to the type of the function is returned if
x equals y.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, z;
long double y;
x = 150.0;
y = 300.0;
z = nexttoward(x, y);
printf("The next representable value after %f in the direction of %Lf is %.10f\n", x, y, z);
x = 150.0;
y = -300.0;
z = nexttoward(x, y);
printf("The next representable value after %f in the direction of %Lf is %.10f\n", x, y, z);
}
Example Output
The next representable value after 150.000000 in the direction of 300.000000 is 150.0000000000
The next representable value after 150.000000 in the direction of -300.000000 is 150.0000000000