6.11.34 copysignl Function
Returns a long double precision value with the magnitude of one value and the sign of another.
Include
<math.h>
Prototype
long double copysignl(long double x, long double y);
Arguments
x- a double precision floating-point value
y- value whose sign will apply to the result
Return Value
Returns the value of x but with the sign of
y.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x,y,z;
x = 10.0;
y = -3.0;
z = copysignl(x, y);
printf("The value %Lf but with %Lf's sign is %Lf\n\n", x, y, z);
}
Example Output
The value 10.000000 but with -3.000000's sign is -10.000000