6.11.51 exp2f Function
Calculates the base 2 exponential function of x
(2x, where x is a single precision
floating-point value).
Include
<math.h>
Prototype
float exp2f(float x);
Argument
x- value for which to return the exponential
Return Value
Returns 2x.
Remarks
A range error occurs if the magnitude of x is too large, and
errno will be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
errno = 0;
x = 1.0;
y = exp2f(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %f is %f\n", x, y);
errno = 0;
x = 10;
y = exp2f(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %f is %f\n", x, y);
errno = 0;
x = -10;
y = exp2f(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %f is %f\n", x, y);
}
Example Output
The base 2 exponential of 1.000000 is 2.000000
The base 2 exponential of 10.000000 is 1024.000000
The base 2 exponential of -10.000000 is 0.000977