6.11.49 expl Function
Calculates the exponential function of x (x, where x
is a long double precision floating-point value).
Include
<math.h>
Prototype
long double expl(long double x);
Argument
x- value for which to return the exponential
Return Value
Returns the exponential of x. Infinity is returned on overflow; 0 is
returned on underflow.
Remarks
A range error occurs if the magnitude of x is too large, and
errno will be set to ERANGE.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = 1.0;
y = expl(x);
if (errno)
perror("Error");
printf("The exponential of %Lf is %Lf\n", x, y);
errno = 0;
x = 1E3;
y = expl(x);
if (errno)
perror("Error");
printf("The exponential of %Lf is %Lf\n", x, y);
errno = 0;
x = -1E3;
y = expl(x);
if (errno)
perror("Error");
printf("The exponential of %Lf is %Lf\n", x, y);
}
Example Output
The exponential of 1.000000 is 2.718282
Error: range error
The exponential of 1000.000000 is inf
Error: range error
The exponential of -1000.000000 is 0.000000