6.11.12 asinf Function
Calculates the trigonometric arc sine function of a single precision floating-point value.
Include
<math.h>
Prototype
float asinf(float x);
Argument
x- value between -1 and 1 for which to return the arc sine
Return Value
Returns the arc sine in radians in the range radians (inclusive) or NaN if a domain error occurs.
Remarks
If x is less than -1 or greater than 1, a domain error will occur and
errno will be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
errno = 0;
x = 2.0F;
y = asinf(x);
if (errno)
perror("Error");
printf("The arcsine of %f is %f\n", x, y);
errno = 0;
x = 0.0F;
y = asinf(x);
if (errno)
perror("Error");
printf("The arcsine of %f is %f\n", x, y);
}
Example Output
Error: Domain error
The arcsine of 2.000000 is nan
The arcsine of 0.000000 is 0.000000