6.11.135 nanl Function
Returns a quiet NaN long double precision floating-point value.
Include
<math.h>
Prototype
long double nanl(const char * tagp);
Arguments
tagp- an optional, implementation-defined string which might be used to represent extra information in the NaN’s significand
Return Value
The call nan("n-char-sequence") is equivalent to
strtold("NAN(n-char- sequence)", (char**) NULL); the call
nan("") is equivalent to strtold("NAN()", (char**)
NULL). When tagp does not point to an n-char sequence or
an empty string, the equivalent call to strtold would have a first
argument of "NAN".
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x;
z = nanl(NULL);
printf("Here is our not-a-number: %Lf\n", z);
}
Example Output
Here is our not-a-number: nan