6.11.74 fmod Function
Calculates the remainder of the division between two double-precision floating-point values.
Include
<math.h>
Prototype
double fmod(double x, double y);
Arguments
x- a double precision floating-point value
y- a double precision floating-point value
Return Value
Returns the remainder of x/y with the same sign as x
and magnitude less than the magnitude of y, or returns NaN if
y is zero.
Remarks
If y is zero, a domain error occurs, and errno will be
set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x,y,z;
errno = 0;
x = 7.0;
y = 3.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
errno = 0;
x = 7.0;
y = 7.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
errno = 0;
x = -5.0;
y = 3.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
errno = 0;
x = 5.0;
y = -3.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
errno = 0;
x = -5.0;
y = -5.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
errno = 0;
x = 7.0;
y = 0.0;
z = fmod(x, y);
if (errno)
perror("Error");
printf("For fmod(%f, %f) the remainder is %f\n", x, y, z);
}
Example Output
For fmod(7.000000, 3.000000) the remainder is 1.000000
For fmod(7.000000, 7.000000) the remainder is 0.000000
For fmod(-5.000000, 3.000000) the remainder is -2.000000
For fmod(5.000000, -3.000000) the remainder is 2.000000
For fmod(-5.000000, -5.000000) the remainder is -0.000000
Error: domain error
For fmod(7.000000, 0.000000) the remainder is nan