6.11.93 islessgreater Macro
Determines if its first argument is smaller than or larger than its second.
Include
<math.h>
Prototype
int islessgreater(floating-point x, floating-point
y);
Arguments
x- any floating-point number
y- any floating-point number
Return Value
Determines if x is smaller than or greater than y, as
if by the expression (x) < (y) || (x) > (y) only without any
invalid floating-point exception should the arguments be unordered (i.e. should one of
them be NaN).
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y;
int b;
x = -5.7;
y = 2.0;
b = islessgreater(x, y);
printf("That %f is less than or greater than %f is %s\n", x, y, b ? "true" : "false");
}
Example Output
That -5.700000 is less than or greater than 2.000000 is true