6.11.153 remquol Function
Calculates x REM y as a long double precision
floating-point value.
Include
<math.h>
Prototype
long double remainder(long double x, long double y, int *
quo);
Arguments
x- a double precision floating-point value
y- a double precision floating-point value
quo- a pointer to an
intobject that can hold the quotient
Return Value
Returns the same remainder as remainder function, being x − ny,
where n is the nearest integer to the exact value of
x/y. In the object pointed to by quo is stored a
quotient with the same sign as x/y, and whose magnitude is congruent
modulo 2m to the magnitude of the integral quotient of
x/y, where m is an implementation-defined integer greater
than or equal to 3. The rounding mode is ignored.
Remarks
If the remainder is 0, its sign shall be the same as that of
x.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x, y, z;
int q;
x = 7.0;
y = 3.0;
z = remquol(x, y, &q);
printf("%Lf REM %Lf is %Lf with quotient %d\n", x, y, z, q);
}
Example Output
7.000000 REM 3.000000 is 1.000000 with quotient 2