6.11.3 Floating-point Classification Macros
FP_INFINITE
Floating-point classification type used by fp_classify,
for example, indicating the value is infinity.
Include
<math.h>
FP_NAN
Floating-point classification type used by fp_classify,
for example, indicating the value is not a number.
Include
<math.h>
FP_NORMAL
Floating-point classification type used by fp_classify,
for example, indicating the value is normal, i.e., it is not zero, NaN, infinite,
nor subnormal.
Include
<math.h>
FP_SUBNORMAL
Floating-point classification type used by fp_classify,
for example, indicating the value is subnormal. Subnormal values are non-zero
values, with magnitude smaller than the smallest normal value. The normalisation
process shifts leading zeros out of the significand and decreases the exponent, but
where this process would cause the exponent to become smaller than its smallest
representable value, the leading zeros are permitted and the value becomes
subnormal, or denormalised.
Include
<math.h>
FP_ZERO
Floating-point classification type used by fp_classify,
for example, indicating the value is zero.
Include
<math.h>
FP_FAST_FMA
The definition of this macro indicates that the fma
function executes at least as fast as the discrete multiplication and addition of
double values.
Include
<math.h>
FP_FAST_FMAF
The definition of this macro indicates that the fma
function executes at least as fast as the discrete multiplication and addition of
float values.
Include
<math.h>
FP_FAST_FMAL
The definition of this macro indicates that the fma
function executes at least as fast as the discrete multiplication and addition of
long double values.
Include
<math.h>
FP_ILOGB0
This macro expands to the value returned by the ilogb
function when passed an argument of zero.
Include
<math.h>
Value
Expands to the value of INT_MIN, as defined by
<limits.h>
FP_ILOGBNAN
This macro expands to the value returned by the ilogb
function when passed an argument of NaN.
Include
<math.h>
Value
Expands to the value of INT_MIN, as defined by
<limits.h>