6.11.148 remainder Function
Calculates x REM y as a double precision
value.
Include
<math.h>
Prototype
double remainder(double x, double y);
Arguments
x- a double precision floating-point value
y- a double precision floating-point value
Return Value
Returns the remainder x REM y, being x −
ny, where n is the nearest integer to
the exact value of x/y when y is not 0. The rounding
mode is ignored. If the remainder is 0, its sign shall be the same as that of
x.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x,y,z;
x = 7.0;
y = 3.0;
z = remainder(x, y);
printf("%f REM %f is %f\n", x, y, z);
}
Example Output
7.000000 REM 3.000000 is 1.000000