6.11.90 isinf Macro
Returns true if its argument is an infinity.
Include
<math.h>
Prototype
int isinf(floating-point x);
Argument
x- any floating-point number
Return Value
Returns true if x is either positive or negative infinity; zero
otherwise.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y, z;
x = 5.0;
y = 0.0;
z = x / y;
if(isinf(z))
printf("Infinity detected in division of %f by %f\n", x, y);
}
Example Output
Infinity detected in division of 5.000000 by 0.000000