6.11.145 pow Function
Calculates x raised to the power y.
Include
<math.h>
Prototype
double pow(double x, double y);
Arguments
x- the base
y- the exponent
Return Value
Returns x raised to the power y
(xy).
Remarks
If x is finite and negative and y is finite and not an
integer value, a domain error will occur and errno will be set to
EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y, z;
errno = 0;
x = -2.0;
y = 3.1;
z = pow(x, y);
if (errno)
perror("Error");
printf("%f raised to %f is %f\n ", x, y, z);
errno = 0;
x = 3.0;
y = -0.5;
z = pow(x, y);
if (errno)
perror("Error");
printf("%f raised to %f is %f\n ", x, y, z);
errno = 0;
x = 4.0;
y = 0.0;
z = pow(x, y);
if (errno)
perror("Error");
printf("%f raised to %f is %f\n ", x, y, z);
errno = 0;
x = 0.0;
y = -3.0;
z = pow(x, y);
if (errno)
perror("Error");
printf("%f raised to %f is %f\n ", x, y, z);
}
Example Output
Error: Domain error
-2.000000 raised to 3.100000 is nan
3.000000 raised to -0.500000 is 0.577350
4.000000 raised to 0.000000 is 1.000000
0.000000 raised to -3.000000 is inf