6.11.114 log10l Function
Calculates the base-10 logarithm of a long double-precision floating-point value.
Include
<math.h>
Prototype
long double log10(long double x);
Argument
x- any long double-precision floating-point positive number
Return Value
Returns the base-10 logarithm of x. If x is 0, infinity
is returned. If x is < 0, NaN is returned .
Remarks
If x < 0, a domain error will occur and errno will be
set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = 2.0;
y = log10l(x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
errno = 0;
x = 0.0;
y = log10l(x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
errno = 0;
x = -2.0;
y = log10l(x);
if (errno)
perror("Error");
printf("The base-10 logarithm of %f is %f\n", x, y);
}
Example Output
The base-10 logarithm of 2.000000 is 0.301030
The base-10 logarithm of 0.000000 is -inf
Error: domain error
The base-10 logarithm of -2.000000 is nan