6.11.94 isnan Macro
Returns true if its argument is NaN.
Include
<math.h>
Prototype
int isnan(floating-point x);
Argument
x- any floating-point number
Return Value
Returns true if x is NaN (not a number); false otherwise.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y, z;
x = 0.0;
y = 0.0;
z = x / y;
if(isnan(z))
printf("NaN detected in division of %f by %f\n", x, y);
}
Example Output
NaN detected in division of 0.000000 by 0.000000