6.11.117 log1pl Function
Calculates the natural logarithm of a long double precision floating-point value plus 1.
Include
<math.h>
Prototype
long double log1pl(long double x);
Argument
x- any positive value for which to return the log
Return Value
Returns the natural (base-) logarithm of x+1 or NaN if a domain error occurs. The result
of log1p(x) is generally expected to be more accurate than that of
log(x+1) when the magnitude of x is small.
Remarks
If x is less than -1, a domain error will occur and
errno will be set to EDOM.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = 2.0;
y = log1pl(x);
if(errno)
perror("Error");
printf("The result of log1pl(%f) is %f\n", x, y);
errno = 0;
x = 0.0;
y = log1pl(x);
if(errno)
perror("Error");
printf("The result of log1pl(%f) is %f\n", x, y);
errno = 0;
x = -2.0;
y = log1pl(x);
if(errno)
perror("Error");
printf("The result of log1pl(%f) is %f\n", x, y);
}
Example Output
The result of log1pl(2.000000) is 1.098612
The result of log1pl(0.000000) is 0.000000
Error: domain error
The result of log1pl(-2.000000) is nan