9.3.6.11 RX_CSRL_REG (in Peripheral mode) Bit Definitions
| Bit Number | Name | Reset Value | Function |
|---|---|---|---|
| 7 | ClrDataTog | 0 | The Arm® Cortex®-M3 processor (or fabric master) writes a 1 to this bit to reset the endpoint data toggle to 0. |
| 6 | SentStall | 0 | This bit is set when a STALL handshake is transmitted. The Cortex-M3 processor (or fabric master) should clear this bit. |
| 5 | SendStall | 0 | The Cortex-M3 processor (or fabric master) writes a 1 to this bit to issue a STALL handshake. The Cortex-M3 processor (or fabric master) clears this bit to terminate the stall condition. This bit has no effect where the endpoint is being used for ISO transfers. |
| 4 | FlushFIFO | 0 | The Cortex-M3 processor (or fabric master) writes a 1 to this bit to flush the latest packet from the endpoint receive FIFO. The FIFO pointer is reset, the RxPktRdy bit (bit 0 of this register) is cleared. FlushFIFO should only be used when RxPktRdy is set. At other times, it may cause data to be corrupted. If the FIFO is double-buffered, FlushFIFO may need to be set twice to completely clear the FIFO. |
| 3 | DataError | 0 | This bit is set when RxPktRdy (bit 0 of this register) is set if the data packet has a CRC or bit-stuff error. It is cleared when RxPktRdy is cleared. This bit is only valid when the endpoint is operating in ISO mode. In Bulk mode, it always returns zero. |
| 2 | OverRun | 0 | This bit is set if an OUT packet cannot be loaded into the receive FIFO. The Cortex-M3 processor (or fabric master) should clear this bit. This bit is only valid when the endpoint is operating in ISO mode. In Bulk mode, it always returns zero. |
| 1 | FIFOFull | 0 | This bit is set when no more packets can be loaded into the receive FIFO. |
| 0 | RxPktRdy | 0 | This bit is set when a data packet has been received. The Cortex-M3 processor (or fabric master) should clear this bit when the packet has been unloaded from the receive FIFO. An interrupt is generated when the bit is set. |