9.2.175 GMAC Express MAC DMA Configuration Register

Name: GMAC_EMAC_DCFGR
Offset: 0x1010
Reset: 0x00020004
Property: Read/Write

Bit 3130292827262524 
   TXBD_EXTENDEDRXBD_EXTENDED TXFOMAXBRXFOMAXBDDRP 
Access R/WR/WR/WR/WR/W 
Reset 00000 
Bit 2322212019181716 
 DRBS[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000010 
Bit 15141312111098 
   CRCERRREPINFLASTENTXCOENTXPBMSRXBMS[1:0] 
Access R/WR/WR/WR/WR/WR/W 
Reset 000000 
Bit 76543210 
 ESPAESMA FBLDO[4:0] 
Access R/WR/WR/WR/WR/WR/WR/W 
Reset 0000100 

Bit 29 – TXBD_EXTENDED Transmit Buffer Descriptor Extended Mode

See GMAC_EMAC_TXBDCTRL for a description of the features.

ValueDescription
0

Disables Transmit Buffer Data Extended mode.

1

Enables Transmit Buffer Data Extended mode.

Bit 28 – RXBD_EXTENDED Receive Buffer Descriptor Extended Mode

See GMAC_EMAC_RXBDCTRL for a description of the features.

ValueDescription
0

Disables Receive Buffer Data Extended mode.

1

Enables Receive Buffer Data Extended mode.

Bit 26 – TXFOMAXB Force Transmit Max Burst Length

Forces the transmit DMA to always issue max length bursts on EOP (end of packet) or EOB (end of buffer) transfers as defined in FBLDO, even when there is less than max burst data bytes to read. Residual data read is ignored. Does not apply to bursts that break 1k boundary rule.

Bit 25 – RXFOMAXB Force Receive Max Burst Length

Forces the receive DMA to always issue max length bursts on EOP (end of packet) or EOB (end of buffer) transfers, even if there is less than max burst real packet data required to write. Any extra bytes of pad data is set to 0x00. Does not apply to bursts that break 1k boundary rule.

Bit 24 – DDRP DMA Discard Receive Packets

When set, the GMAC DMA will automatically discard receive packets from the receiver packet buffer memory when no system memory resource is available.

When low, the received packets will remain to be stored in the GMAC local memory packet buffer until system memory buffer resource next becomes available.

A write to this bit is ignored if the DMA is not configured in the packet buffer Full Store and Forward mode.

Bits 23:16 – DRBS[7:0] DMA Receive Buffer Size

DMA receive buffer size in system memory. The value defined by these bits determines the size of buffer to use in main system memory when writing received data.

The value is defined in multiples of 64 bytes, thus a value of 0x01 corresponds to buffers of 64 bytes, 0x02 corresponds to 128 bytes etc.

For example:

0x02: 128 bytes

0x18: 1536 bytes (1 × max length frame/buffer)

0xA0: 10240 bytes (1 × 10K jumbo frame/buffer)

Note that this value should never be written as zero.

Bit 13 – CRCERRREP CRC Errors Report

ValueDescription
0

Bit 16 of the receive buffer descriptor represents the Canonical format indicator (CFI) bit as extracted from the receive frame (if the receive buffer descriptor is pointing to the last data buffer of the receive frame and the received frame was VLAN tagged).

1

Bit 16 of the receive buffer descriptor represents the FCS/CRC error (only if frames with FCS are copied to memory as enabled by bit 26 in the Network Configuration register).

Bit 12 – INFLASTEN Infinite Size for Last Buffer Enable

Set to ‘1’, this forces the receive DMA to consider the data buffer pointed to by the last descriptor in the descriptor list to be of definite size.

Bit 11 – TXCOEN Transmitter Checksum Generation Offload Enable

Transmitter IP, TCP and UDP checksum generation offload enable. When set, the transmitter checksum generation engine is enabled to calculate and substitute checksums for transmit frames. When clear, frame data is unaffected.

Bit 10 – TXPBMS Transmitter Packet Buffer Memory Size Select

This bit at zero halves the amount of memory used for the transmit packet buffer. This reduces the amount of memory used by the GMAC. It is important to set this bit to ‘1’ if the full configured physical memory is available. The value in brackets below represents the size that would result for the default maximum configured memory size of 4 Kbytes.

ValueNameDescription
0 TWO_KB

Do not use top address bit (2 Kbytes).

1 FOUR_KB

Use full configured addressable space (4 Kbytes).

Bits 9:8 – RXBMS[1:0] Receiver Packet Buffer Memory Size Select

The default receive packet buffer size is 8 Kbytes. The table below shows how to configure this memory to FULL, HALF, QUARTER or EIGHTH of the default size.

ValueNameDescription
0 EIGHTH

8/8 Kbyte Memory Size

1 QUARTER

8/4 Kbytes Memory Size

2 HALF

8/2 Kbytes Memory Size

3 FULL

8 Kbytes Memory Size

Bit 7 – ESPA Endian Swap Mode Enable for Packet Data Accesses

ValueNameDescription
0 LITTLE_ENDIAN

Selects Little-endian endianism for system bus transfers.

1 BIG_ENDIAN

Selects swapped endianism for system bus transfers.

Bit 6 – ESMA Endian Swap Mode Enable for Management Descriptor Accesses

Selects the burst length to attempt to use on the system bus when transferring frame data. Not used for DMA management operations and only used where space and data size allow. Otherwise system bus single type accesses are used.

ValueNameDescription
0 LITTLE_ENDIAN

Selects Little-endian endianism for system bus transfers.

1 BIG_ENDIAN

Selects swapped endianism for system bus transfers.

FBLDO: Fixed Burst Length for DMA Data Operations:

Bits 4:0 – FBLDO[4:0] Fixed Burst Length for DMA Data Operations

ValueNameDescription
0 – Reserved
1 SINGLE Always uses single access on system bus
2 – Reserved
4 INCR4

Attempt to use 4-beat bursts on system bus (Default)

8 INCR8

Attempt to use 8-beat bursts on system bus bursts

16 INCR16

Attempt to use 16-beat bursts on system bus bursts

50