5.49 Block Erase_64KB (BE_64KB)

The Block Erase_64KB (D8H) instruction clears all bits within the selected 64-KB block to 1. If the command targets a protected memory region, the erase operation is ignored. Before starting any write operation, the WREN command must be executed. The CE# signal must remain active-low throughout the entire command sequence. To execute a Block Erase_64KB operation, the host drives CE# low, issues the Block Erase command (D8H), transmits three address bytes, and then drives CE# high. Address bits [AMS–A16], where AMS denotes the Most Significant Address, specify the target block address, while the remaining address bits may be set to either VIL or VIH. Completion of the internally timed Block Erase_64KB operation can be confirmed by polling the Busy bit in the status register or by waiting for the specified TBE64KB interval. Refer to Figure 5-42 and Figure 5-43 for the Block Erase command sequences.

Figure 5-42. Block Erase Sequence (SPI)
Note: MSb = Most Significant bit
Figure 5-43. Block Erase Sequence (QPI)
Note: MSN = Most Significant Nibble; LSN = Least Significant Nibble, C[1:0] = D8H