13.33.211 timer_set_maxdelay

Adds a maximum delay constraint to the specified path.

timer_set_maxdelay -from source_pin \

-to destination_pin \

[-unit {value}] -delay delay_value

Arguments

-from source_pin

Specifies the name of the source pin in the path.

-to destination_pin

Specifies the name of the destination pin in the path.

-unit {value}

Specifies whether the delay unit is in nanoseconds or picoseconds. The following table shows the acceptable values for this argument:

ValueDescription

ns

Sets the delay in nanoseconds

ps

Sets the delay in picoseconds

-delay delay_value

Specifies the actual delay value for the path.